800xA for MOD300 Connectivity Server UseGlobalAck
Hi All ,
I would like to know if anyone knows anything about
the purpose of the "UseGlobalAck" registry key in a 800xA for MOD300
Connectivity Server .
Is it something related to alarm and event management
in a mixed environment with Advant for MOD300 consoles
and 800xA clients.. ?
Any answer will be appreciated.
Thanks a lot
Paul.
Answers
UseGlobalAck = 0 by default i.e Only Local Acknowledgement and No Global ack.
when this value is zero operators need to ack the alarm on each console seperately wherever alarm is presented.
if it is set to 1 then alarm can be acknowledged from one place and it will acknowledge in all operator stations.
Remember this setting is not for normal 800xA alarms but MOD300 Message Centre alarms such as CCF_Alarm, TCL_events.
I suggest to change the value to 1.
Add new comment