Modbus TCP error
I am using a CI867 as modbus TCP slave, it has 3 masters connected and they have a 1.1 seconds, 970ms and 1 second interval request.
Sometimes the masters loss the connection with the CI867. When I check the log file, for the CI modules I find the following error:
"Trying to decrement memory counter below zero", this error is repetitive everyday, and after some time the controller flushes the memory queue and resets the CI867 module, that is what I understand of the log file.
I wonder if there is something I can configure in order to prevent that "filling queue" or "memory counter filling"?
Attached the portion of the log file.
Thanks.
Answers
This question has not yet been answered.
Add new comment