MODBUS TCP for freelance
Do you know if Modbus TCP will be released for Freelance and when?
Thanks
Voted best answer
Modbus TCP is in the testing right now. It is scheduled to be released with the next Freelance version by end of Q1/2013
Answers
Dear Csanchez,
With current versions it is possible to communicate over Modbus TCP with freelance using gateways/convertors as freelance supports MODBUS RTU/ASCII, Nevertheless if you are looking for integrated MODBUS TCP solution with freelance controller then, it will get release .., Answer of when you can get from marcom channels
Add new comment