Why a full backup is not working and it stay waiting
My system have a 6.0 version, and I am trying to do a full backup, but this operation is not start.
Answers
Hello,
so you mean that no Backups are created in Maintenance Structure ?
Verify the service provider under Service Structure, BackupService.
Is the service running (Status tab).
The Special Configuration tab shows where to store the backup.
Do you have enough space left ?
Is the free space limit over free space left on the device ?
The Service Account is running the backup.
Do you have a domain or workgroup ?
Sin otro particular
/Ronny
Add new comment