AC800M Project library expand and alarm 2 same lib in project
I were create new project from exist one where project were saved to same project-forder by save project as and project were split in 2
Other had only Application and Controller folder other had Controlmodules etc like normally.
and now it was giving that alarm: Two identical lib ....
It look that this start to apper if project are saved by : Save project as
and then it is big job to arrange libs. again so that no warning appear ... and then if you copy project to other PC some of files might be missing and can't open project.
Q1. Is there any rules or correct way to do reveision ''backup'' during work ..
I had previously used to made BAckUp to different folder with folder by dates ...
Q2. Is there any easy way to fix this 2 same folder issues ... instead error/try method ...
thanks ....
Answers
Hi,
Described by you is known problem for me too.
It will be interested to see if any usable advise will come to your question.
Usually I copy the libraries (my own libraries, both SW and HW) to the project folder. Then use Insert Library to include the library to the project, then rename the library.
With a new name there is no "duplication" problem (you need to re-open CBM).
In this way, finally, you can just copy your project folder and have all the necessary files, if open on the other PC.
Other good option is a project backup from CBM Tools-> Maitenance-> Project Backup.
It creates copy of all used files, which you can move and use on the other PC.
Add new comment