WEB Display on Freelance ver 9.2 SP1
Hello,
I am trying to call up an IP camera but there is no respons on the PC.
The PC is W7.
If I give the IP address direct in the PC, via IE9, it works fine but when
I send the same command via a button nothing happens.
I have somthing in my head that you must do something in the PC
but I can´t find anything in the documentation.
Can anyone help me.
Thank you.
Best regards
Tore Wassén
Answers
Hello Tore
there are 2 ways
A) Configure a Web-Display for DigiVis that contains the URL to the camera's Web-Server
B) Configure an External Aspect in the Display Access
Solution B requires a license for the External Aspect, while the Web-Display license is part of a standard FO license lately.
Add new comment