sms is not going to more that one number
I have configured SMS and when the alarm is generated SMS is going only for the first number of message handle.
Answers
Set timeout = 0 in the Message Handler aspect.
I sometimes need to disable Apply en enable Apply again in the Message Source tab to make it work.
Try giving delay option between numbers. Dont prefer to send message to all numbers all together. Its possible in Message handler.
Add new comment