How to create two Alarm lists for two PLCs in one Server in CHMI compact 800.
Hi Expert,
Currently i'm using CHMI compact 800 with 1 server and 2 PLC program.
Now i wanted to create 2 alarm lists for each of the PLC program. means alarm list 1 only show the alarm from PLC_1. and alarm list 2 only show the alarm from PLC_2.
Any idea?
Thank you.
Answers
Put one alarm list aspect in the control structure on each of plc1 and plc2 and configure them to show only objects and descendants.
You can also easily filter on some alarm attribute, e.g. Class, Severity, etc.
/Stefan
Add new comment