UMC 100 Configuration - Freelance
Hi,
I'm having trouble configuring UMC 100 GSD into Freelance. First I've inserted UMC100-FBP (R0101 R0201) into the node and then I went to IO editor to configure the modules of communication (Figure 1), and that is the problem.
When I start to insert the inputs, the number of bytes that I need is smaller than the available(Figure 2).
I think that I'm using the wrong type of configuration when I'm inserting the modules. I could not find the memory map to make the correct configuration. Am I doing something wrong?
Thank you.
Voted best answer
DTM also available for UMC100 R0102 version.UMC100 R0102 integration is successful with freelance system. You have control application builder also to use with the device.
Control application builder have device specific funtion block for usage.Following is the device type for UMC100 with PDP you can download the same from solutions bank or ABB library for usage. Read the release notes first to know about the issues and workarounds during integration if any.Let us know your feedback for the same.
2PAA108677S01_C_en_Freelance_ABB_PDP22-FBP_UMC_100_DTM_Library_5.2.2_0.exe
Add new comment