Adding System functions to Existing system in 800xA 6.0.3
I restored 800xA 5.1 Maintenance backup in a freshly installed 800xA 6.0.3 system, by deleting the new system created during installation. But during restore, a warning was thrown which said- the following extensions are missing
-Engineering Platform
-Function Designer
-ABB PC, Network and Software Monitoring System Extension
-Topology Designer
-DM & PM Application
-SCSystemExtension
Because of this, a few graphic elements in the screens are missing.
I found out that these missing extensions are part of Asset Optimization and Engineering Studio. So i need to add these functions to redundant server nodes (Primary and Secondary ASCS). But I'm not sure whether the existing license package includes license for Asset optimization and Engineering studio.
Please refer the attached screen shots of license entry and confirm the same.
Also, please let me know whether it is possible to add new functions to existing primary and secondary server (running system) without doing a fresh installation on all nodes.
Answers
Attachments (license entry)
Hello
None of above product belong to AO. You need PNSM system extension but license (AO_NET_MON) is not required if you use only Basic PNSM functionality. So it is safe to load.
For other products you have Engineering studio license.
I dont know what is SCSystemExtenstion (I guess its Script Manager from Engg studio).
I think you are good to install system extension.
Add new comment