AI895 Configuration - Freelance
Hi,
It is my first time configuring the AI895 card into freelance (using CI801 with profibus). Inside my application I've configured the value read from the card using a INT variable + UINT block converter + AINT block (4-20 mA), but I've got problems with the AINT output value.
What I want to know :
1. The AI895 always uses INT? It is possible to configure to another data type?
2.Do I have to do any configuration on the hardware tree?
Thank you
It is my first time configuring the AI895 card into freelance (using CI801 with profibus). Inside my application I've configured the value read from the card using a INT variable + UINT block converter + AINT block (4-20 mA), but I've got problems with the AINT output value.
What I want to know :
1. The AI895 always uses INT? It is possible to configure to another data type?
2.Do I have to do any configuration on the hardware tree?
Thank you
Voted best answer
Hello Willians,
Yes S800 I/O’s using INT data type, nevertheless you need not have to struggle with data type for your usage, you can use available FB from export folder.
From your PC go to CFB\Edit\Import block and browse at this location C:\Program Files\ABB Industrial IT\Freelance\export\S800_UFBs_US and use SAI8XX block. you can use this block for AI810,AI845,AI895.
Also FB available for S900 I/O & ACS800 drive.
Hope it helps to you.
Add new comment