CM50 Communication with freelance over modbus
Looking for solution of CM50 Single Loop Controller interfaced with Freelance AC 800F over modbus communication.
Answers
I have tried to interface freelance AC 800F with CM50 over Modbus RS485, It was interfaced successfully find attached here with quick setup guide, project csv including UFB library and other details.
Pls note that incase exporting UFB library for usage or while using this UFB in different project configure MODM_DEV object name as "CM50_MOD" so that plausibility check will not through error for wrong interface object.
Check associated app @ http://www402.abbext.com/Freelance-connect-with-CM-over-Modbus-rtu-Application-
CM-backup-to-Freelance-DCS_1-0_a364.aspx
Source:
Add new comment