Differences between PP865 and PP865A
Anyone there who knows this ?
Thanks
BR
Voted best answer
Please have a look in the ABB library too.
Search for Product Updates and Bulletins.
All panels will have new CPU and power boards and some models will have new energy efficient TFT-displays with LED backlight. The panels will be one to one replaceable and there is no change in the Panel Builder 800 configuration tool. The new panels will keep certifications like UL 508, DNV, GL etc. However, they will no longer be UL 1604 (Class 1 Div II) certified.
The panels will get new article numbers as well as new type designations:
3BSE042239R1 PP815 will become 3BSE042239R2 PP815A with new display.
3BSE042243R1 PP820 will become 3BSE042243R2 PP820A.
3BSE042240R1 PP825 will become 3BSE042240R3 PP825A with new display.
3BSE042244R1 PP826 will become 3BSE042244R3 PP826A with new display.
3BSE042234R1 PP835 will become 3BSE042234R2 PP835A with new display.
3BSE042237R1 PP836 will become 3BSE042237R2 PP836A with new display.
3BSE042235R1 PP845 will become 3BSE042235R2 PP845A.
3BSE042238R1 PP846 will become 3BSE042238R2 PP846A.
3BSE042236R1 PP865 will become 3BSE042236R2 PP865A.
Note: The panels are delivered with panel firmware which supports the new hardware; do not downgrade a panel with a firmware older than the preinstalled.
Answers
Hi!
PP865A has a rechargable battery.
Add new comment