Fuzzty logic implementation
anybody worked with fuzzy logic in Control builder ???
If so please help me with an example ...
Answers
Hello,
Fuzzy logic can be configured using a standard library named 'ControlFuzzyLib'. All standard blocks are avaialble in that library.
There is a separate sub-section (named 'Fuzzy Control') under Section-4 of the manual '3BSE035981-510_A_en_System_800xA_Control_5.1_AC_800M_Binary_and_Analog_Handlin
g.pdf' which explains the configuration of the fuzzy logic.
Also, refer: Appendix-B of the same manual for information about the functionalities of the library blocks.
Add new comment