About Industrial IT
I want to know in About Industrial IT dialog box from where it reads the product & version?
Voted best answer
The about box lists system extension info from the System Extension info aspect on the system's domain object in the Admin Structure.
Unfortunately, the naming convention is not very easy to understand.
For day to day identification of what you have installed; I sincererly recommend to read installed products and versions from the Control Panel -> Programs and Features.
However, Programs and Features will not tell if the system extension has also been loaded into the 800xA system, or is just ready to be loaded. This info must be derived from the System Extensions aspect (or the About... box).
/Stefan
Add new comment