How connect faceplate to extended info (MOT1 - BMI Library)?
I need to add a link in the second button of the extended information section in MOT1 of Minerals Library.
This button is configured in Control Build M (Extended Info = 64), but I not found the option to add link.
Thanks.
Voted best answer
The Link is to the Parent Object in Control Structure, like if you create a new Control Module with its own Faceplate and include a MOT1 in it.
If you want to change this, either override the "BMI Overlap Link" Aspect on the MOT1 or the Faceplate itself and configure a different Link.
Add new comment