"Project Contains an old target model no longer supported. Project can not be opened." ?
This message comes up for me after having downloaded and installed the Panel Builder 800 program yesterday, when I try to open projects. All of these projects are valid projects that colleagues of mine, with exactly the same version of software, are able to open without issue. The only option after receiving this message is to return to the opening program dialog.
Answers
All of the projects have been created with a later version of Panel Builder, and were using an unrecognized panel. This version of Panel builder was therefore unable to work with them.
Unfortunately, Panel Builder 6.0 doesn't support older Panels 800, e.g. PP865, PP845 etc.
It is intended only to program the new panles from ver. 6 - eg PP871, PP874...
For older panels you have to use Panel Builder 800 ver. 5.x which support them.
There are other posts in AKS about that
Add new comment