For 800xA 5.1 is missing bulk data manager sheets that where in 5.0 (CBM_xxxx.xls). Where are they?
In 800xA 5.1 there are less bulk data manager sheets than in 800xA 5.0
The following sheets are missing (but very welcome to have in 5.1):
- CBM_Applications.xls
- CBM_ControlModules.xls
- CBM_ControlModuleTypes.xls
- CBM_FunctionBlockDiagram.xls
- CBM_FunctionBlocks.xls
- CBM_FunctionBlockTypes.xls
- CBM_HWUnits.xls
- CBM_IO_Variables.xls
- CBM_Programs.xls
- CBM_SingleControlModule.xls
Does anybody know if there are replacements or if there is a solution to upgrade the 5.0 BDM-sheets yourself to 5.1 sheets (because they are not all compatible)?
Answers
Hello,
For your information,
In RN system 800xA 5.1 rev B it is mentioned that some Bulk Data Manager templates available in earlier versions prior to 800xA 5.1 are obsolete.
Hope it helps to you...
Find those templates in associated app.
Add new comment