Freelance Controller Emulator Administrator Page
I am using Freelance CBF 2013 Demo version, I am facing problem of "No connection" during the commissioning mode. even though I enter the resource ID, and then I can't "shutdown" the Emulator and processors from the administrator page, when I press shutdown icon, the Station No. still appearing. I tried to enter/change to different different ID but still facing the problem.
For Info. I restarted the PC several times, and disabled the antivirs and firewall.
Really Appreciate your assistance to fix this issue.
Answers
Please check with Task mananger whether a msrntvc.exe process is active; you can enable the command line column in Task manager to see the startup parameters.
You can terminate the the msrntvc.exe processes from the Task manager and try to start it from a command line window: in the exe directory run "msrntvc -i 2 -a 127.0.0.1 -d 10002 -g 10003". This will start an emulator for resource id 2, giving console output.
Add new comment