Integrating a third-party OPC AE (alarms and events) server in 800xA 5.1
Say I have a third-party (Kepware) OPC AE server running on a server that is outside the 800xA domain and want to connect it to the 800xA system...
As far as I can tell from the documentation (3BDS011222-510_F_en_System_800xA_5.1_Configuration.pdf p. 460-), this should be possible.
Will I be able to get these alarms in my existing 800xA alarm lists? How do I define the alarm class?
Also, can PLC connect be utilized with OPC AE? I'm only familiar with OPC DA.
Answers
I have attached the documents How to configure. Please go through and Let me know if you need more INFO.
Add new comment