Which version of 800xA with this build number?
Hi,
Could anyone help me for this build number ?
ABB 800xA Base: 5.1-0
Build number: 204005780
Thanks.
Voted best answer
We generally try to avoid using build numbers to identify and distinguish between different system versions. Even within the same version, multiple build numbers exist and may cause confusion: a)System extension build number (one per system extension!) b) Windows installer package build number (one per software component!) I'm not sure, but I believe a Temporary Correction may affect both a) and b) so, generally speaking - try to avoid using build numbers for identification purposes. Where did you find this number? I assume from a) a) can be derived from the System Extensions aspect (see below from a 5.1 FP4 system that has passed through FP1->FP2->FP3->FP4)?
The b) build number may be selected for presentation in Programs and Features
Or be read from the C:\Program Files\ABB Industrial IT\Operate IT\Process Portal A\Process Portal A.log installation log file: Process Portal A distribution package =====================================================================Package built with : Aspect Studio (Version : 5.10.4139.16247)Name : ABB 800xA Base S-FP 5.1.4Publisher : ABBVersion : 5.10.4797.33138 <=============== My ESX server is down for maintenance (storage extension) so I can't view my "revision track" machines, but I assume "204005780" is 5.1 RevB or 5.1 RevC (it is not 5.1 RevA). Will update this thread when I know more.
/Stefan
Source:
Answers
Hi,
You have noted down the build number from the Admin structure under the system extensions aspect. I am not aware of any document with which you can refer this build number to get the exact system version.You need to go to the ADD remove programs and then click on the softwares with name "ABB 800xA base" and you will get the product version information.Note that down and you can use the product version information with the technical description document
3BSE056732-System 800xA 5.1 System Software Versions, to get the exact deails.Ofcourse if you have used any temporary corrections then you will not find the details about the temporary correction in the document and need to consult the local support orgnization for the same.
You can check your version in cmd command:
C:\dir
Add new comment