UFB freelance property different in objet type structure than functionnal structure
Hello, i'm using a user block function in ac800f whit 160 property.
In 800xa Object type structure all property is present but in the functionnal and control structure many property are missing.
Is there a limit for number of property we can using for ufb ?
Voted best answer
Hi Can you please explain your question in more detail.
Regards
Answers
In controle connection,for a object type i can see in control connection "Property view" that all properties Name are corresponding at the properties declared in FB-CLASS of control builder F. But in control and functionnal structure in "control connection" two properties are missing. It's the same for all user defined function blocks of the project.
You can find screnn shot in attached file.
Regards.
Add new comment