What is the optimum screen resolution to use in developing and running graphics to make sure the des
Answers
The screen resolution should be the same on the machine, where pictures are built, as on machines where pictures are used. Recommended resolution is 1280 x 1024 pixels.
Add new comment