Freelance don´t find the hardwarekey
Hello.
I have a ver 9 system where I have changed to a new PC, W7.
When I try to install the licens Configure say it´s OK, successfully installed
F2k-file.
The LED in the hardwarekey is on but still CBF and DigiVis starts in Demo.
I have restared the PC and I have used different USB.
Can anybody help me with a solution?
Best regards
Tore Wassén
Answers
Hello Tore,
the Hardkey must plugged in during installation of Freelance in Production mode.
No Hardkey => Demo mode will installed.
A change from Demo to Produktion needs to deinstall Freelance and install it with Hardkey plugged in again (select Production mode).
Best regards
Bernd
Sorry Tore,
the answer of Bernd is not correct.
It is not necessary to reinstall the software.
Normaly it works fine. Is it the right hardkey for the F2k-file?
You can find the hardkey number inside the F2k-file.
Best regards
[123456789]
0=6C6A2DDE1A86B10346E3EE0D1A6E8805DB9A83F0213CCA6BE815DE61BABB2EFA
;DIGIVIS,10,3,*,1
1=C50CE2CFD1409B7CA9346E94557A58D292DA6C54EA093BA77AB68D0C0041D927
;DIGIVISSTD,10,3,*,1
2=8211731276CEA9B86D3E5B12832F5BEC0170D00C3F052E993C3795038A2367B5
;FGR_COUNT,10,3,*,5
3=9472153A28D447D937DD4A2B3BC6712F6EC6DBD8A4282A82993B22D35CBF31C9
;MULTIFPL,10,3,*,5
4=5CF0AA3DE2CAD121AD2301EE6C7E363E2391BEBBAF72BD135DE9A41CC2048A19
;SIGNALCOUNT,10,3,*,NOL
5=1397126DFA49B86FF30D23BF4A83CDC6DB9A83F0213CCA6BE815DE61BABB2EFA
;VIS_IMS,10,3,*,1
6=3415936BC2A99F3C3F5447B9807A4EBC97DEA0026F1B076D7AB68D0C0041D927
;WEBDISPLAY,10,3,*,1
This is an example of a F2k-file
[123456789] is the Hardkey number.
The number must be identical.
What about the system requirements.
You talk about a version 9.
W7 is released since version 9.2 SP1 for W7 32bit
and since 9.2 SP2 for W7 64bit
Add new comment