System without workplaces
Operate IT 1.2 Beta 3: I installed the package with the default options (i.e. without the Graphics Builder), and I got no workplaces at all! No errors about this, and the server could be started, but no way to start or create any workplaces. The solution was to re-install the software WITH more options (I think the key was the Graphics Builder), and then create the system again.
Answers
Please, read answers to my question at previous Topic: AIP1.0-1 without VB ???
The main thing is that you should have at least visual basic installed in the machine to get any workplaces in AIP 1.0-1 (or Operate IT 1.2)
The main thing is that you should have at least visual basic installed in the machine to get any workplaces in AIP 1.0-1 (or Operate IT 1.2)
Add new comment