Change System Name
I want to change the name of a system, and tried to do it by changing the value of the system under the "ABB|Sigma|Systems" key in the registry. The new name is accepted and displayed in the configuratin wizard during startup. But at some point during the start up, the registry name is reset to the original name. Where do I have to change the system name?
Answers
Some entries inside the Aspect Directory are mirrored peridically into the registry.
I changed "[Admin Structure]Administrative Objects/Domains/MyMachine System" from "MyMachine System" to "NewSystem".
After the next startup, the new name showed up.
I changed "[Admin Structure]Administrative Objects/Domains/MyMachine System" from "MyMachine System" to "NewSystem".
After the next startup, the new name showed up.
Add new comment