Does the Cross Reference list work for control modules ?
I installed the entire Engineering Studio in a 800xa system version 3.1 SP2 (with the rollups).
My applications uses only Control Modules and when I use CBM_CrossReferences.xls template, it only generates the list of variables in the "Programs" part of CBM.
Do I have to setup something in particular to have the cross references of the variables included in the control modules ?
My applications uses only Control Modules and when I use CBM_CrossReferences.xls template, it only generates the list of variables in the "Programs" part of CBM.
Do I have to setup something in particular to have the cross references of the variables included in the control modules ?
Answers
To get all references you have to press also another button "Get Cross References for All Variables" in worksheet "Editor".
But before this button is enabled you must have pressed button "Create Variable List" and then go back into the worksheet "Editor" again.
But before this button is enabled you must have pressed button "Create Variable List" and then go back into the worksheet "Editor" again.
I did that and the result is only variables that are in the "program" part nothing from the Control Module" part.
Add new comment