how to extract the input output listing from 800xA ver 4.1.
how to extract the input output listing from 800xA ver 4.1. That is , i want to get the inputs and outputs connected to I/O modules in word/excel format.
Voted best answer
Hi!
Import source code (.BAX or .BA) into Excel as text. Filter out the information you want. If you are good at writing macros, then automate it.
Answers
Theres also an export function in Control Builder A which can create one file per database element type. This imports directly to MS access or excel without writing macros.
At some point, there was a complete AC400 control project database tool written in MS Access by ABB singapore. You might still be able to track down a copy somewhere.
by MichaelStarc Rank: 350 on 3/2/2014 4:21:19 AM | Like (0) | Report
In AC450 controller
Add new comment