insert aspect of the object in graphics is through insert element in control structure and using graphics option i
Voted best answer
Every object uploaded from an AC450, has aspects. Some of the aspects are of the object type Graphic Element. Theese can be inserted into Graphic Displays.
Depending on version of your system you are using VB or PG2 to build your displays. The technique is the same, browse for object in control structure (or any other structure where the object is located) using the element browser. Choose aspect, insert!
Add new comment