How to import "metso positioner ND9000 v5" DD file in Freelance 800F ver 8.2
Dear Sir
we have a problem with assigning a metso ND 9000 V5 positioner to ABB freelance 800F V8.2,We already had a metso ND 9000 V2.1 positioner and now we want to replace it with v5 we also provide the dd file from metso but when we are trying to assigning it the following error will occur,is there a procedure to assigning the dd file correctly ?in which directory should I copy the dd file folder? How should assign it with to CBF 8.2!?
please help us if someone knows about this problem.
Voted best answer
You need to update the capabilities file in the parameter dialog of the FF_DEV_CLASS object. The parameter dialog has a Capabilities File tab, which has an Update button.
But upadte possibilities are limited. If the device description differs, a new device class needs to be created.
Hope that helps
by Flavio Mussolin
Sorry
I'm not so expert in AC800 series
by Dieter Henkel
I don't see any error message attached.
by Govindaraj
Edited by Admin: Error Image added.
Add new comment