How can I find out MOTCON database complete terminals details in AC450 controller.
DATABASE TERMINAL DETAILS
=217.31:121/MMC_X.781FN1:121
=217.31:94/MMC_X.781FN1:94
=217.31:10/MMC_X.781FN1:10
DATA BASE CROSS REFERANCE
MOTCON MMCX2/781FN1
AB_FILE# I PC5.12.2.3:7
ION I PC5.12.2.10.100:2
F_SIZE O PC5.12.2.10.100:21
PC_PARM I PC5.12.2.10.110:PARAM
PC_RES O PC5.12.2.10.110:RESULT
MORD O PC5.12.2.10.140:O
Answers
Have you checked in the standard documentation?
I searched the Advant OCS with Master Software User Documentation CD-ROM which returned multiple hits on the keywords you listed above (I did not search for all of them though).
My CD has article number 3BSE008143R1201
/Stefan
by admin Rank: 29 on 2/24/2014 8:28:23 PM | Like (0) | Report
Pls continue in same question thread if you have further question via comment to answer section.
Deleted new question asked by you in relation to this question and added text from there to comment section here in answer.
Cheers
-Admin
Add new comment