CI855 library in Control Builder M?
Where can I find CI855 hardware library for control builder M?
Does not seem to be included in standard installation.
Answers
[Object Type Structure]Object Types/Control System/AC 800M\/C Connect/Libraries/Hardware/CI855MB300HwLib 2\.1-2
Quick find:
Nothing there.... found only the same libraries that showed in Connected Libraries in Countrol Builder M.
In Control Builder -> Libraries -> Hardware ->Right Click and select Insert Libray
Then select the requested Library - e.g. CI855MB300HwLib-2-0-4.hwl
After insert the library in the project, you have to connect it to the requested controller
Add new comment