Hello Everyone, I am using Un licenced (free) version of Freelance 2016. Are there any limitations for OPC tags?
Hello Everyone, I am using Un licenced (free) version of Freelance 2016. Are there any limitations for OPC tags?
I have configured more than one PLCs in OPC configurator but im not able to recieve OPC tags for All of them. Are there any limited number for OPC tags for syncronisation in free version of Freelance 2016. because when I syncronise OPC item list. it only show OPC tags from 2 PLCs.
Answers




Hi asad1837,
As far as I know there is no limit for OPC TAGs in demo version of Freelance.
I think that there is some problem with the names You are using as I don't understand what You mean and how can I help You. What do You mean by: "I have configured more than one PLCs in OPC configurator"? What is "OPC configurator"? And how did You configured PLCs in it? What is more what do You mean by "OPC tags"? OPC variables or OPC faceplate (so called OPC_TAG_Types)?
I will make a guess based only on last sentence of Your question - You are trying to connect PLCs (like AC 500) to Freelance by means of OPC, but when syncing OPC server You can see data from only two PLCs.
If that is the case then You most probably have a problem with OPC server configuration or its connection to PLCs.
Please answer the questions above, so the community can help You accordingly.
Best Regards,
Mike
by asad1837 Rank: 585 on 2/21/2017 3:17:53 AM | Like (0) | Report
I have configured more then two PLCs in OPC configurator.
Add new comment