PM583 Utilize COM2 for transmitting application data
Greetings,
I have a PM583. After the PM583 is programmed, I need to connect a serial cable to COM2 port and send custom ASCII strings with custom runtime information. Is this possible? If so, where can I find an example project or tutorial guide on performing this feature in CoDeSys?
Answers
Attach is the example connection AC500 with PC Hyperterminal.
The details and cable pinout is inside the project.
Add new comment