In xA 5.1 Functional block like or, move are mulfunctioning..!
Version:- 800xA 5.1/0
Bmi Library:- 5.1/3a
Controller:- PM864
OR gate and Move gate are not giving output even if the inputs are true
Answers
Please ensure that these blocks are enabled for execution and the outputs are not over written in any other logics. These are basic function blocks and almost no chance of malfunctions in these.
No chance of malfunctioning of these standard modules.See read/write status of variables which are written by these modules they can be written simultaneously by different commands.
does the program have an assigned task
Add new comment