Operation and engineering station freezes in Freelance 9.2
I have a station of engineering and operation with the freelance 9.2 but the virtual memory of the station with windows 7 x32 this station of saturation and the station this is freezing after some days the computer the restart and returns to function normally, the Digivis Running On the administrator session by the Freelance user sells a Watchdog error when it is opening and does not allow to start.
Answers
Hi,
You say the station is "freezing". Please tell us more.
Does the mouse cursor stop moving?
Does the Digivis clock stop counting?
Does the Digivis graphics stop changing?
Does the station become slow or sluggish?
Does the harddisk stop working?
Does the harddisk acting normal, short access every few secends?
Does the harddisk acting like crazy, are they busy?
Does the station restart without your action?
You suspect the virtual memory use going to saturation. This information is useful, but not precise. We need to know which process takes all the memory. Please write down the memory consumtion of all processes, and compare after some hours. Repeat this until you know the process who increases memory consumption all the time.
(By the way memory leaks of applications should not lead to freezing the whole station. Typically this temporary slow down the station and finally crash the application only.)
by JuergenV Rank: 71 on 2/8/2017 11:05:23 PM | Like (1) | Report
Dear Rafael,
Can you tell which process has had the high memory consumption? Is there also an OPC gateway on that machine?
Best regards
Jürgen
by Rafael_Valerio Rank: 2139 on 2/8/2017 11:34:31 PM | Like (0) | Report
A lot of cache data is generated when I open the digivis, there is only the opc of the stations there is another operating station that does not present any problem
by Rafael_Valerio Rank: 2139 on 2/9/2017 3:43:07 PM | Like (0) | Report
Send photos of the configuration:
https://drive.google.com/file/d/0B-EEq8P5wgCIM25CeS1WeXE4QzQ/view?usp=sharing
https://drive.google.com/file/d/0B-EEq8P5wgCIV1dwRWRwUFQzZzA/view?usp=sharing
Thank you
Add new comment