800xA Operator workplate (operator login) - shrinked workplace
We are using ruggedised laptops for mibile operator work stations.
Operator workstation correctly opens up in full screen of the laptop when logged in as engineer ot admin. But does not open up in full screen (as attached) for operator and viewonly user instead it shrinks in size on opening.
800xA Version 6.0.2
All running Windows 8.1, 16GB memory
Just to be honest on this, I have raised a Supportline case as well, This question on AKS is to see if any one has the same issue and if there is a known fix for this.
Answers
Have you checked affected user's Microsoft Windows setting for font scaling?
To increase readability (but without altering screen resolution) you can change font scaling, eg 100% -> 150%
It is a lesser known fact that System 800xA require this setting to be left at 100%.
Add new comment