Scaling the SR100B and adding an offset probem
Niki Good day I do install the SR100 B to read the load of a motor I do mange to scale the analog signal (Electrical & engineering ) what I could not mange to do is how to: 1- Expand the recorded chart over the chart paper (i.e. now i to loading curve of the motor vary between the first Colum of the chart paper and the third ... what i want to do is to expand that so I want the curve at the full load to be at the 2- I try to add existing Colum offset or change the span but is did not mange to ... i just follow the steps in the user manual .... is there anything else i should take care of kindly advice Regards
Voted best answer
You can adjust how much of the chart is used by using the chart scaling configuration parameters in the menu. this allows you to set up how much of the chart is used. However it does have limitations and is not as flexible as the 'zoming' functionality of the Paperless chart recorders.
Source:
Add new comment