Query about license uses if controller is changed?
We have a system in which PM856 controller is there.
we want to upgrade the system using only PM861 Controller. None of the configuration will be changed except controller.
Does the license depend on the controller?
or we can use the same licence with the new controller?
we want to upgrade the system using only PM861 Controller. None of the configuration will be changed except controller.
Does the license depend on the controller?
or we can use the same licence with the new controller?
Voted best answer
Hello,
In 5.0 SP2 vesrions licensing on Control&I/O depends upon CLP's (I/O based)
In SV 5.1 versions,the licensing is depends upon CCP (Controller Capacity points) - It varies depends upon Controllers (AC800M_QUANTA)
If you are using Controller based license, then you need to purchse new license for PM861.
Refer 3BSE047441_I_en_Wizard_800xA_User_Manual_Additions fro more details.
Add new comment