PP835 Single Alarm Acknowledge Not Working After PM856 Boots from CF Card
We use AlmCondBasic blocks in Compact Control Builder to generate alarms which are displayed on a PP835 HMI. When we first download the application programs to both devices, the "defaul" Alarm Acknowledge (Single) button on the HMI works fine. However, when we cycle power to the AC800M PM856 and PP835 HMI, the single alarm acknowledge button no longer works.
Answers
Pls cycle power on the panel too. Might need to restart the TCP communication. Or report the issue to our support line.
Add new comment