Is it possible to remove the frames from a quad/dual panel operator workplace display?
I would like to display multiple graphics on the one screen, but without the surrounding frame with pin/zoom/etc. buttons.
Ideally I would like a split screen (rows) and retain the frame on the top screen.
Is this possible?
Answers
Hi,
Yes,It is possible follow below mentioned steps>
Library struture>Default aspect>Graphic Display>select Main View(Aspect)>select property Override:In General property change frame visible to "False"
WR,
Lohith
Add new comment