AC500 errors
Could you point me in the right direction in how to solve the following errors? What manual should I look in?
E3 026
d1 014
d2 255
d3 003
d4 000
Thank you,
Rob
Voted best answer
Hello Rob
while using Automation Builder/CoDeSys, if you open the help file you can look for error codes and see what the program suggests.
For example, the error E3 indicate the class of error (minor error) and the number 026 indicate config data.
If you search inside the help file the string
you can read the definition of errors and in the string
the type of errors
Hope this help you
Add new comment