Batch transition failed to execute
Hi,
This question in relation to Batch Management 800xA SV 5.1 FP4.
In batch procedure, operator message flag is set in the phase and reset from PFC.
During batch run time, transition fails with error message.
transition expression error unitattget bmsGetUnitAtt (unit=UN_R_523 Attribute=R523_MAG_OM1_Set).
or
Operator message error---Error:UN_T_612:OM1_Flagg write failed: Blk ID 26:Compute expr; error Expression.
OPCCACHE_E_ 0x80040c03 WriteTimeout:Unwritten:PH_612_O:OM1_Flagg
The Problem is resolved when the equipment attribute is removed and created again. However, I want to know what causes this problem in first place and how it can be solved permanently.
Thank you in advance
Answers
This question has not yet been answered.
Add new comment