OPC Funtion Block Classes for Freelance
I know with the Control builder F Professional you can create "OPC Funtion Block Classes", but I supouse that Control builder F Standard and Control builder F Professional include a OPC Funtion Block Classes standard library, the question is for wich ABB controllers and 3rd Party PLCs exist OPC Funtion Block Classes standard (including in the base license of the Control builder F)?
In reference to the ABB controllers I almost sure exist a OPC Funtion Block Classes for AC500 (PLC), but I don't know if exist some for AC800.
In reference to 3rd Party PLCs I need to know The Brand (Siemens, Rockwell, schneider, hima,etc) and wich models of PLC of this brand (Siemens S7-200, Siemens S7-300, Rockwell MicroLogix 1200, Rockwell MicroLogix 1500,Rockwell SC500, etc)
Answers
Hello Eurits,
I think you have question regarding OPC Tag Type Library(OPC Function block library OPC_FB-LIB)? You can find AC500 standard and Freelance sample tag type library @ "C:\Program Files\ABB Industrial IT\Freelance\export" path on your freelance V9.2 7572 SP1 install based computer. This is available with even demo freelance software.
Add new comment