Audit events in the Event List of 800xA ?
I would like to have registered in the event list the operator's log in to the system 800xA.
Anybody would know if this is possible? and how?
Voted best answer
800xA can not know when a user logs into Windows; this has to be queried to the Windows Event Log.
However, by enabling the AuditEvent_System, 800xA will log an audit event when a workplace starts and stops normally (I believe an abnormal stop may not result in any event)
By creating a custom event list with attribute filter for Message its quite easy to create an event list that only lists workplace start/stop and not the other events that may arrive on the same category.
Or the event list can be made to filter on Objects and Descendants in the Workplace Structure.
/Stefan
Answers
Hi Boris
I believe that adding / check "Simple Events"->"Operation" to the Alarm and Event List Configuration aspect concerned will do it.
BR Carsten
There is also possibility under security environment:
Check document 3BSE037410-510 D.
Add new comment