AC800F demo mode
English version : google translated
Good afternoon I would like to inform about the monitoring software for AC800F builder. Currently I have the software in demo mode for 100 days, but if you can do some downloading to the controller without a license. I watched the tutorial and upload an app to be going the way of man icon commissioning of the helmet, but when I select that button closes the application, do not know if I have something wrong or permanently installed without license I can not make downloads and testing with real equipment. In addition to this, I can not add DTM Profibus slaves, to add an AO card for Profibus remote I had to install the gsd CI830 module, this is also due to demo mode?.
thank you very much
Spanish version :
Buenas tardes me gustaria informarme sobre el software control builder para el AC800F. Actualmente tengo el software en modo demo por 100 dias, pero no se si se puede realizar alguna descarga al controlador sin tener la licencia. He visto el tutorial y para poder cargar una apliación se debe ir al modo comisionamiento del ícono del hombre con el casco, pero cuando selecciono ese botón se cierra la aplicación, no sé si tengo algo mal instalado o definitivamente sin la licencia no puedo realizar descargas y realizar pruebas con el equipo real. Adicionalmente a esto, no puedo agregar esclavos profibus DTM, para agregar una tarjeta remota de AO por profibus tuve que instalar el gsd del módulo CI830, esto también es debido al modo demo?.
Muchas gracias
Voted best answer
Hello,
If I understood correctly, you have freelance installed in demo mode and it is not possible to go in comissioning mode and not possible to add profibus slave DTM. If so
Regarding DTM, CI801 and CI840 profibus slaves are selectable/supported via DTM. there is no relation with demo and licensed version.
The function is same in both demo/licensed version, so even in demo mode it is possible to download to controller.
Want to confirm did you downloaded freelance software in demo mode first time on that computer ? or before there was licensed version and you have downloaded software in demo mode now ? Which freelance version you are using ? If it's your first time with freelance recomended to go through getting started manual available in demo dvd. or
Hope this helps
Answers
Hi,
If i understood correctly,
Question 1: Unable to download the application in demo mode?
Ans: Create the application in CBF, go to "Project" menu available in main menu and select "Commissioning", R.click on Process station-> select load whole station.
Note: Download to controller is possible in both demo and licensed mode.
Question 2: Unable to add Profibus DTM slaves?
Ans: Please check whether you insatalled FDT DTM components, if not please install by selecting "Modify" option during installation.
Please provide Freelance version which you are using...
I hope this helps you...
by admin Rank: 29 on 10/7/2013 6:55:19 PM | Like (0) | Report
Edited by Admin:
Hello to help in getting answer translated text into English language and recomended to use English language to get fast and more answers.
Add new comment