Communication between AC500 and CAN BUS Slave
Hello, I want to implement a CAN bus communication between an AC500 PLC and a CAN BUS subscriber. I have a CM578 communication card but I can not declare a CAN BUS protocol, I have access only to CAN OPEN protocol. I have unfortunately no experience in this fieldbus. Could a person help me on this? The only information I have from the CAN BUS subscriber is a * .dbc file. I'm working on version 1.2 of Automation Builder with Codesys 2.3. Thank you in advance for your help
Answers
Hi
you can start reading the application note for AC500 and CAN BUS, download at the follow link:
http://www.abb.com/abblibrary/downloa...
Hope this help you
Unfortunately the example provided is based on a CANOpen communication. CANBUS management in CODESYS is different.
Add new comment