Create eventlist in 800xA for Windows events sent via SNMP traps
Hello,
I am trying to create an eventlist that works with the PNSM IT Device Traps aspect to show me events that I forwarded via SNMP. I got the SNMP part working fine but I can't figure out how to make 800xA recognize the traps and put them into an eventlist. I already deactivated the native Windows services and activated the ABB Trap receiver. I wrote the necessary MIB files and imported them into the Device Trap aspect. But i cant figure out how to create the eventlist properly.
I'd appreciate any help.
Thank you very much in advance.
Voted best answer
Begin with creating an unfiltered event list; do the trap events appear there?
The simple event category for which you can filter for is:
- ITAssetTrapMessages_ABB 800xA System Message Server
If no such events are found in the system, there is probably some problem with the PNSM Trap Receiver and/or setup of SNMP (e.g. firewall).
Add new comment