Writing Advant Unix OS Backup to CD
Hello,
Is it possible to write the Station Backup of Advant Unix Operator Station on a CD.
Please advise the unix commands for writing.
The station is B2000.
Answers
I am sure by using the Tape drive we can have the backup of the unix machine. But i dont think so, we can write the backup directly to the CD or DVD from B2000 machine. Because CD writer function will not be there in UNIX machines.
Else you can transfer the files or backup from B2000 /B2600 machines and u can write in CD / DVD.
CoreFTP is the tool which we can use to transfer the files from UNIX based mchines...
Regards,
Prabhakaran D
Hello,
I think this will be a challange for more than one day. The allmost knoen way to make a backup / restore of an OS is by using tape. (old school)
I guess that the commands using the backup and restore task only work with tape devices. I think it is more simple to use an old SCSI Tape device to backup or restore the operator station.
But anyway good luck.
Michael
Add new comment