EI813F Ethernet Module battery part number
Hi :
I'm looking for the lithium battery part No. for an EI813F ethernet module.
Does anybody know where to look for that Part no.????
BR
Fausto
Voted best answer
I've just ordered some few weeks ago from our stock myself.
The part number is 3BDM000199R1, it's called "SB 808F". Each ordered item includes 2 batteries.
Answers
Think it's this one
If you are looking for other options, here is a Google Search (I am in the US, so this should show US Vendors), that you can check. There are several vendors that you can find where you can source the battery, including the brand that you are currently using.
https://www.google.com/webhp?sourceid...
Another option is to go to a local battery store, if there are any in your area, like Batteries Plus or Battery One Stop. Take the old unit in and if they do not have them in stock, they should be able to order in that unit or an equivalent.
ABB outsources the batteries, obviously, so you do not need to use exactly that battery, just one with the same or better specifications.
Good luck.
Rob Murphy
Add new comment